Use Periodic Interrupt at MR_CANHUBK344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use Periodic Interrupt at MR_CANHUBK344

1,017 次查看
236
Contributor I

I want to use periodic interrupt function.....

Help me please....

I use S32DS 3.4.

0 项奖励
回复
2 回复数

976 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

There is Pit_Ip_example_S32K344 example in S32K3 RTD 2.0.x.

See also S32K3xx PIT and STM with RTD - Training


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,016 次查看
236
Contributor I
And my porject is based on "MR_CANHUBK3_IEEE1722" project.
0 项奖励
回复