Use EB tresos config SPI module: set SpiCsBehavior but code does not changed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use EB tresos config SPI module: set SpiCsBehavior but code does not changed.

999件の閲覧回数
RyzeBai
Contributor I

Hi,

As shown in the screenshot, set NO.0  and NO.1 Devices SpiCsBehavior 1.

But code shows only Device1 has changed.why?  

My RTD  is SW32K3_RTD_R21-11_3.0.0_P07

RyzeBai_0-1726109970827.png

RyzeBai_1-1726109985188.png

 

0 件の賞賛
返信
1 返信

964件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @RyzeBai,

I'm not able to reproduce it using the Spi_Transfer_S32K344 (RTD_R21-11_3.0.0_P07) example in Tresos 29.

Can you share the whole project, or a test project that can replicate the issue?

 

Regards,

Daniel

0 件の賞賛
返信