Hi
The 128-bit unique identification number is loaded into IFR during manufacturing process and it is set for each device as identifier of the device and placed into our internal records about device.
Even different variants will not have the same 128-bit unique identification number.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------