Unable to load sample project-S32K1xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to load sample project-S32K1xx

1,264件の閲覧回数
Sundar_96
Contributor I

Hello,

I downloaded and installed the RTM for S32K1xx: S32K14X_MCAL4_0_RTM_1_0_0. When I try to load the sample project into my EB Tresos studio V21.0.0, I get this error: "Plugin with a module xxx_TS_T40D2M9l0R0 is not installed - cannot create module configurations for project sample_app_mcal_s32k14x".

 

Please help me solve the same.

-Sundar

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,223件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hello @Sundar_96.

Please refer to the "AUTOSAR_MCAL_SA_UM" documentation. This document provides a series of steps in order to correctly install and build the sample application. You can find it at the following path: C:\Freescale\AUTOSAR\S32K14X_MCAL4_0_RTM_1_0_0\Sample_Application\doc.

Please note that MCAL for S32K1xx devices is already in End-of-Life status. If further support is required please reach out to your NXP representative for further support.

Please let me know if this information is useful.

- RomanVR.

Best Regards!
0 件の賞賛
返信

1,215件の閲覧回数
Sundar_96
Contributor I

Hello @RomanVR ,

I followed the steps as mentioned in the document provided. But, when I try to load the configuration in EBTresos studio, I face the error, which I had posted originally in this discussion.

Please let me know the next steps regarding the same.

 

With best regards,

Sundar.

0 件の賞賛
返信

1,172件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hello @Sundar_96.

I apologize for the inconveniences but as this is an End-of-Life version, any error or bug may not be addressed or fixed. If you require to use this software version, please reach out to your NXP representative for further support. 

However, we highly recommend transitioning to the latest software versions (EBtresos 29.0) along with the RTD packages. These provide a wider variety of module example projects which are also AUTOSAR 4.4 and 4.7 compliant.

- RomanVR.

Best Regards!
0 件の賞賛
返信