USB-ML-UNIVERSAL-FX burn S32K314 error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-ML-UNIVERSAL-FX burn S32K314 error

597 Views
sunflower11
Contributor I
Dear all,

USB-ML-UNIVERSAL-FX burn S32K314 error, regardless of whether the target board
is connected or not, displays the attachment same error. already tried to set
it according to the "S32K3xx Secure Debug Support" ,but still displays the same
error. and the reset pin of the USB-ML-UNIVERSAL-FX always at low level.
The same target board can be burned successfully by replacing it with another
USB-ML-UNIVERSAL-FX. Could you help to advise what should we can set it? thank
you.

Operating System: Windows 10 Enterprise Edition
software:S32 Design Studio for S32 Platform 3.4
error.png
0 Kudos
Reply
2 Replies

579 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it looks as the issue with the Multilink itself, especially if you tried different one and it works properly.
Check if the ribbon cable is placed properly within Multilink. Also consider driver/firmware version and if needed ask PEmicro support directly.

BR, Petr

0 Kudos
Reply

564 Views
sunflower11
Contributor I

Hi, Petr,

thanks for your advice and will try to check driver/firmware.

Best Regards,

Tina

0 Kudos
Reply