I want to generate ADC drivers for S32K344 using S32DS IDE for non-autosar. After going through the RM I have understood that there is a hardware trigger for conversion using the TRGMUX. Instead, for normal conversion mode, is there a way to trigger the ADC conversion periodically (with a timer). Is there any configuration to do this inside the ADC configurations in the code generator itself.
解決済! 解決策の投稿を見る。
Hi
Please refer to:
Example S32K344 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300
Example S32K344 PIT BTCU ADC DMA DS3.4 RTD100
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Is there an example without using BCTU. Instead using a periodic interrupt for Normal conversion mode
Hi
Please refer to:
Example S32K344 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300
Example S32K344 PIT BTCU ADC DMA DS3.4 RTD100
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------