Tresos example project for S32K148

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tresos example project for S32K148

ソリューションへジャンプ
2,739件の閲覧回数
drsn
Contributor I

Hi, 

   I couldn`t find any example project for Tresos. I have download several MCAL versions to check this. Inside of installation folder for MCALs(C:\NXP\AUTOSAR\S32K1XX_MCAL4_0_RTM_1_0_5) there is no example project. Only the plugins available. 

  It is same situation for RTD, it has only plugins there is no example. How can I find the Tresos example for S32K148? 

 

0 件の賞賛
返信
1 解決策
2,656件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.

If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.

The examples for SW32K1_RTD_4.4_1.0.1 are located in:

:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148

Similar in folders for each driver.

For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.

There are much more examples.

Best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,727件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, that is strange.

I have just installed version S32K14Xx_MCAL4_0_RTM_1_0_0 and sample application is there:

petervlna_0-1681300834814.png

Usually the sample applications are in the base releases.

Best regards,

Peter

0 件の賞賛
返信
2,721件の閲覧回数
drsn
Contributor I

Hi Peter, 

   Thank you for the answer. Yes sample application is only available in base version. but now I have a problem while opening the project in Tresos. sample project uses "xxx_TS_T40D2M9I0R0" version plugins but I have "xxx_TS_T40D2M10I0R0" with base version. It seems that sample project is using older version. Do you know where can I find this version? 

Best regards

0 件の賞賛
返信
2,657件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.

If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.

The examples for SW32K1_RTD_4.4_1.0.1 are located in:

:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148

Similar in folders for each driver.

For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.

There are much more examples.

Best regards,

Peter

0 件の賞賛
返信