Transmitting data via SPI dma s32k324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transmitting data via SPI dma s32k324

Jump to solution
4,231 Views
ann14
Contributor II
I have been using SPI DMA for data transfer with the digital pins IC in S32K324. While the data transmitted is generally correct, we are encountering instances where incorrect data is transmitted.
 
Our analysis indicates that the MOSI line does not start sending data immediately upon clock enablement. This results in an additional bit (1) being added to the data, which affects the integrity of the data being transmitted.
 
I have attached screenshots that illustrate this issue for your reference.
Correct transmission of dataCorrect transmission of data

 

Clock and MOSI line is synchronized correctlyClock and MOSI line is synchronized correctly

 

Incorrect transmission of dataIncorrect transmission of data

 

Slight delay in the MOSI line on clock enablementSlight delay in the MOSI line on clock enablement

 

SPI_DMA_IT_Clk_MOSI_Synch.png

 

0 Kudos
Reply
1 Solution
4,101 Views
ann14
Contributor II
Hi @Senlent
It is working now after changing it from leading to trailing. Thank You for the help.

View solution in original post

0 Kudos
Reply
12 Replies
4,201 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

You can have a try to increase PCSSCK .

Senlent_1-1744102628841.png

PCSSCK parameters correspond to SpiTimeCs2Clk

(Please ignore the configuration in the picture, I just want to tell you where to set this parameter)

Senlent_2-1744102829189.png

 

4,195 Views
ann14
Contributor II
Hi @Senlent,
according to the datasheet of the IC being used the chip select to clk time is 100ns. I gave this value and did the analysis but still it showed the same results.
0 Kudos
Reply
4,186 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

“according to the datasheet of the IC being used the chip select to clk time is 100ns”

I think 100ns should be the minimum allowed value, not the maximum value.

Because I can't tell the actual PCSCLK value from your picture, you can measure the actual PCSCLK value.
Then change the value of SpiTimeCs2Clk and send me a screenshot of the test result.

4,183 Views
ann14
Contributor II
Hi @Senlent
You are correct the minimum value for the cs to clk is 100ns. But while testing we had varied the value of cs to clk from 100ns to the maximum value that is possible. Yet still the results where the same. If you would like i could provide you with the further result illustrations
0 Kudos
Reply
4,149 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

Yes,please, also could you please tell me which version of RTD you are using and show me the I2C parameter configuration in your S32 DS.

0 Kudos
Reply
4,134 Views
ann14
Contributor II

Hi @Senlent ,

I am currently using RTD 3.0.0 and SPI DMA configuration. I have attached the logs taken along 

SPI_Settings.pngSPI_Settings_2.pngScreenshot 2025-04-09 091725.pngScreenshot 2025-04-09 092340.pngScreenshot 2025-04-09 092654.pngScreenshot 2025-04-09 092919.pngScreenshot 2025-04-09 093646.png

0 Kudos
Reply
4,108 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

Senlent_1-1744191048743.png

According to the MC33972 data sheet, I think you have set it wrong here.

I have change it to TRAILING.

Senlent_0-1744191032872.png

 

0 Kudos
Reply
4,085 Views
ann14
Contributor II
Hi @Senlent
From this timing diagram how were you able to identify that data is sampled on the trailing edge.
0 Kudos
Reply
4,052 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

From this timing diagram, this should be sampled from the falling edge of SCK, not the rising edge.

0 Kudos
Reply
4,102 Views
ann14
Contributor II
Hi @Senlent
It is working now after changing it from leading to trailing. Thank You for the help.
0 Kudos
Reply
4,129 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@ann14

Thanks for your detail info, aslo,please share the slave device you're using, i want to see if there is anything that can be improved.

0 Kudos
Reply
4,125 Views
ann14
Contributor II
Hi @Senlent
MC33972ATEWR2 this is the slave device we are using
0 Kudos
Reply