Tolerance of LPIT CVAL (Current timer value)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tolerance of LPIT CVAL (Current timer value)

ソリューションへジャンプ
8,467件の閲覧回数
Hozumi
Contributor I

Regarding the CVAL (Current timer value) of NXP S32K144 LPIT, TRM states that "may not return the true value during operation"
However, could you clarify the tolerance of the values returned during LPIT running?

The lower bits of CVAL are truncated according to the required timer accuracy, so if the tolerance is within the truncated range, it can be used as the Current timer value.

0 件の賞賛
返信
1 解決策
8,439件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,
This weakness is caused by limited functionality on the internal synchronization gasket between LPIT’s bus interface block and peripheral functional clock.
It’s not possible to provide max expected difference between the reads because it depends on the particular bit that hasn’t yet transitioned to the correct value.
To identify potentially wrong read of the CVAL, it’s recommended to use triple vote method.
Regards,
Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
7,716件の閲覧回数
parth_rastogi10
Contributor III

Hi Lukas,

Regarding the reading of the CVAL of LPIT Driver, apart from reading in the ISR section which is already mentioned as the workaround for the errata the triple vote method is suggested to get the correct CVAL values. So, is this triple vote also can be added to the Errata workaround as an alternate solution for the CVAL Errata.

Please respond to the above query as soon as possible by tomorrow as it is an urgent need for the project.

Thanks,

Parth Rastogi
0 件の賞賛
返信
7,701件の閲覧回数
parth_rastogi10
Contributor III

Hi Lukas,

Can you please respond to the query that I posted for the workaround for reading CVAL.

@lukaszadrapa 

Thanks,

Parth Rastogi
0 件の賞賛
返信
8,455件の閲覧回数
Hozumi
Contributor I

On the otherhand, TRM (Rev. 12.1, 02/2020) states that "At any time, the current value of the timer for any channel can be read by reading the corresponding channel's CVALn register. The M_CEN bit must be '1' when doing so." in 48.5.2 page1549.

What are the conditions under which the LPIT CVAL does not return the correct value?

0 件の賞賛
返信
8,440件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,
This weakness is caused by limited functionality on the internal synchronization gasket between LPIT’s bus interface block and peripheral functional clock.
It’s not possible to provide max expected difference between the reads because it depends on the particular bit that hasn’t yet transitioned to the correct value.
To identify potentially wrong read of the CVAL, it’s recommended to use triple vote method.
Regards,
Lukas

0 件の賞賛
返信
8,362件の閲覧回数
vienpeng
Contributor II

Hi, @lukaszadrapa, could you please introduce "triple vote method" in detail ? Is it  a 100% solution ?

0 件の賞賛
返信
8,326件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

triple vote method means that you perform three consecutive reads and then evaluate the result. If there's uneven value, discard it.

The reads should be done as fast as possible. If it is done by CPU, use critical section, so no interrupt is triggered. Another option is to use DMA.

I got information that the possibility to read wrong value is higher if ratio between peripheral clock and bus clock is lower. If the ratio is 1/24, at least, it can still occur but probability is smaller and triple vote will eliminate the problem. Or, as already mentioned, use the same clock source (but triple vote is also needed).

Regards,

Lukas

 

0 件の賞賛
返信
8,196件の閲覧回数
Hirofumi
Contributor II

Hi, Lukas

About your comment "possibility to read wrong value is higher if ratio between peripheral clock and bus clock is lower"

Please tell me why this problem occur ?

0 件の賞賛
返信
8,429件の閲覧回数
Hozumi
Contributor I

Hi Lukas,

Depending on the relationship between the bus clock and the LPIT's count clock, can we read CVAL correctly?
For example, bus clock = LPIT's count clock.

0 件の賞賛
返信
8,414件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

If the LPIT’s bus interface clock and peripheral functional clock are derived from the same clock source, it can significantly reduce the problem. However, it's not 100% solution. Still the triple vote should be used.

Regards,

Lukas

0 件の賞賛
返信