There is a microsecond level delay when capturing the input signal of S32K142W chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There is a microsecond level delay when capturing the input signal of S32K142W chip

1,149 Views
FAR1234
Contributor III

Dear NXP experts,

Background of the problem:
MCU: S32K142W;
Application background: Configure FTM2 as capture mode to capture three-phase Hall signals for BLDC motor control.
Problem description: Adding an instruction to reverse GPIO at the input of the FTM2_Ch0uCh1_IRQHandler() interrupt function, it was found that the capture trigger time can be delayed by up to 3.2us compared to the captured signal. I only set the interrupt priority of "FTM2_Ch0_Ch1_IRQHandler" to the highest priority 0. As shown in the following

figure:

FAR1234_0-1760317897831.png

CH1 channel (yellow waveform): FTM2 captures interrupt reversal IO port;
CH2 channel (blue waveform): periodic square wave generated by the signal generator;

My FTM2 configuration is as follows:
Configure reference information, refer to this image:

FAR1234_1-1760317954566.png

Specific configuration information of FTM2:

FAR1234_2-1760317995122.png

FAR1234_3-1760318019862.png

Looking forward to your reply, thank you.

LF

 

 

 

0 Kudos
Reply
2 Replies

1,111 Views
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

Could you please share you project using Real Time Drivers (RTD) and compatible with the S32K14WEVB-Q064 (or any other of our EVB) in order to reproduce your issue from our side?

In addition to the ICU configuration, please also add the necessary PWM settings to test all the issue in a single board. And any extra details that are necessary please.

Thank you in advance for details.

0 Kudos
Reply

1,063 Views
FAR1234
Contributor III

Hi @_Leo_ 

I am glad to receive your reply.

Regarding your question, the response is as follows:

1, S32 Design Studio for S32 Platform Version: S32DS v3.4

2, SDK: S32SDK_S32K1XX_STM_4.0.3;
3, MCU:FS32K142WAT0WLFT;

4, For the input capture routine of Hall signal, I built it myself according to the prompts in the NXP user manual. For specific configuration, please refer to my  last message.

5,Tested PWM signal properties:
Frequency: 20KHz;
Duty cycle: 50%;
High level voltage: 5V;

Best Regards

LF

0 Kudos
Reply