The range of RTC compensation value S32K148

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The range of RTC compensation value S32K148

1,674 次查看
SONGTAOSI
Contributor I

Hi,

According to the reference manual, the range of the time compensation value is-127~128.However, When i configuring 128 to the  time compensation value, the following error occurs,it  out of range.

SONGTAOSI_0-1677650398173.png

 

Can you give me some suggestions? the reference manual is not right?

 

 

0 项奖励
回复
2 回复数

1,656 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SONGTAOSI

The content in the data sheet is not wrong, and the setting range here is -128~127, and there is nothing wrong with it. The reason for the difference is that the 8-bit binary highest bit is signed.

0 项奖励
回复

1,652 次查看
SONGTAOSI
Contributor I

Hi,

thank you Senlent.

what should this range be when I set it in the project?

const rtc_init_config_t rtcTimerInitCfg0 = {
.updateEnable = false,
.nonSupervisorAccessEnable = true,
.compensationInterval = 0U,
.compensation = 127, // What would be the range here? -128~127?
.clockSelect = RTC_CLK_SRC_LPO_1KHZ,
.clockOutConfig = RTC_CLKOUT_SRC_TSIC
};

 Thank you again.

0 项奖励
回复