The difference between FX32K and FS32K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The difference between FX32K and FS32K

4,720件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hello, 

     If the full P/N of FX32K and FS32K have the only difference on 'X' and 'S', these two chips could be pin-2-pin compatible on hardware. The only difference for SW should be taken care on the default value of SDID register. Detail of SDID could be checked on S32K1xx reference manual. 

    FX32K and FS32K use the same data sheet and reference manual.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

Cheers!

Oliver

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,780件の閲覧回数
KLMan
NXP Employee
NXP Employee

if the only differnet is X and S, SDID should be exactly same since they are identical part, am I correct?

0 件の賞賛
返信

3,603件の閲覧回数
LucasPirola
Contributor I

Inside the S32K-DS.pdf is attached an excel files with the Orderable Part Numbers for S32K microcontrollers, and as of Rev. 10, this file does NOT include any part number starting with FX32K.  This led to confusion and time consuming activities in my team. This information now seems stable enough to be added to the list and avoid further confusion.

0 件の賞賛
返信