T-BOX S32K148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T-BOX S32K148

1,577 Views
1971439734
Contributor II
hi everybody! i have a problem, i can't connect MCU. try many times. I just have j-link. so how to solve this?? Connecting to J-Link... J-Link is connected. Firmware: J-Link V9 compiled May 17 2019 09:50:41 Checking target voltage... Target voltage: 3.33 V Listening on TCP/IP port 2331 Connecting to target...ERROR: InitTarget(): PCode returned with error code -1 ERROR: InitTarget(): PCode returned with error code -1 ERROR: Could not connect to target. Thanks. best wishes.
0 Kudos
Reply
1 Reply

1,563 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer the method described in: S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决

Hope it helps.

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply