Dear Sanket,
1. Does NXP provide a standalone evaluation GUI or PC software for the MC33774A?
[A] Yes, there is an EvalGUI 7 for the MC33774A. Specifically to be used with RD33774ADSTEVB. The GUI is intended to be used with SPI interface for communication between MCU and SPI to TPL transceiver and then via TPL to the MC33774A. Please refer to the UM11816.

If you are asking if there is a GUI specifically for the RD33774CNC3EVB with populated MC33665A TPL to CAN transceiver for the communication with MCU via CAN interface, unfortunately, there isn't any.
2. Is there a FreeMASTER project, demonstration GUI, or any other graphical tool that can be used to monitor and configure the MC33774A through the BMU?
[A] For the BMU and CMU boards you mentioned we have a whole software bundle. However you need an S32DS IDE.

Please refer to this link. Included are Demo projects for the FreeMASTER.

Please refer to the Release Notes document on the right side.

3. Is there a reference application or example firmware that enables evaluation of the MC33774A with minimal software development?
[A] See above what software is available for the EVBs you have. However, the two boards are not sufficient. You need your own battery pack, with minimally 4 Cells for each MC33774A, or we have BATT-18EMULATOR. Emulating 18 Cells for each MC33774A populated on the RD33774CNC3EVB.
Please refer to the UM11943.


4. Are there any applications describing the recommended setup for evaluating the MC33774A using only the BMU and CMU evaluation boards?
[A] Yes there is. However as mentioned above you need either a battery pack or the battery emulator. Please refer to the UM11943 and to this link.

With Best Regards,
Jozef