Simulate I2S on S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulate I2S on S32K144

1,959 Views
yuliucao
Contributor I

Hi,

I want to setup a system which supports 2 channel input and 6 channel output on S32K144.

There was an example in SDK, but it only has 2 Channel input and 2 Channel output.

My system will look like:

  • FlexIO pins configured as SCK, WS, IN1, OUT1, OUT2, OUT3
  • Sample Rate: 48kHz
  • I2S format

Please let me know if this is possible and do we have example code available?

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies