Setting up freemaster in second core.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up freemaster in second core.

764 Views
RChatterjee
Contributor III

Hi,

I want to setup the freemaster in the M7_2 core of s32k358,with the rest of my communication peripherals. but i can't attach the project to that core for some reason. How do I resolve this.

Also, in a different post I had read that both cores have access throughout the whole ram, so there should be no issuesin making such an configuration, right?

0 Kudos
Reply
1 Reply

728 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @RChatterjee 

It is not possible to attach FreeMASTER SDK to the Core 1 since the communication between cores and FreeMASTER should bee made through the Inter-Platform Communication Framework (IPCF). For a better understanding for multicore communication with FreeMASTER refer to S32K324 Triple PMSM Software. 

S32K324 Triple Permanent Magnet Synchronous Motor Control (PMSM) Reference Design Board

 

B.R.

VaneB

0 Kudos
Reply