SPI Interrupt Enable Register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Interrupt Enable Register

626 次查看
qiansan
Contributor I

Will setting the SPI ier to TDIE position 1 cause the SPI controller to send an interrupt request to the NVIC;1.png

0 项奖励
回复
1 回复

620 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi qiansan,

You can see the condition that triggers the interrupt from the section 51.3.1.5 Status Register (SR) and 51.4.4 Interrupts and DMA Requests of S32K1xx MCU Family - Reference Manual

.TDF 51.3.1.5 Status Register (SR).png51.4.4 Interrupts and DMA Requests.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复