[SM_070] SW register test within FTTI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[SM_070] SW register test within FTTI

2,036 Views
Catosh
Contributor IV

Hi all, 

I need a clarification about SM_070 in SM rev.4 :

[SM_070] The safety-relevant configuration registers shall be checked at least once per FTTI to verify their proper content.

and  the related reccomendation: 

Using application software, periodically check the contents of configuration registers (more than 10 registers) of modules attached to the PBRIDGEs to help detect faults in the PBRIDGE.

the implementation hint states that 

The following safety integrity functions for register configuration checks are recommended in this document. Depending on the application, you can choose to check them differently or can consider other peripherals as per safety

and the modules are Flextimer(s), port(s), adc, pdb and lpit. 

In the attached HW_Safety_Measure_reactionTime I can see that also SCG SW register is expected to be check. 

My question(s) is(are): 

  • is sufficient to check the registers of the recommended modules + SCG from the iso26262 perspective or NXP in the FMEDA evaluation expects ALL registers to be checked? 
  • The reccomendation about PBRIDGE requires to check periodically the configuration of the registers in AIPS-lite OR to perform [SM_070] on ALL peripherals (if safety relevant, obviously)?

K.R.

Luca

0 Kudos
Reply
1 Reply

1,523 Views
Kive
Contributor I

Hello Catosh,

Do you mind sharing the implementation of the CRC check for the registers?

0 Kudos
Reply