SHIELD COMPATIBILITY with S32K148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SHIELD COMPATIBILITY with S32K148

1,523 Views
marin_visciano
Contributor I

Hey guys, I'm Marina. I'm using this board : s32k148evbq176, I need to know if this GD3000 3PHASE BRUSHLESS MOTOR PRE-DRIVE is compatible with pins-out of my board. If it is not compatible may you show one that is good for my board? 

Tags (2)
0 Kudos
Reply
1 Reply

1,454 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, Mariana 

Could you please confirm if you refer to this shield Low-Cost Motor Control Solution for DEVKIT Platform | NXP? If so, then yes, it is compatible with the evaluation board you are using. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply