SCST Tests interrupted in the first atomic test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SCST Tests interrupted in the first atomic test

1,665 次查看
aymane_chaib_nxp95
Contributor I

Hello,

I am working in a program for automtive use, the code is bellow:

static void mst_SCST_RunGroup(const mst_stScstGrpDesc_Type *pstScstGrp)

{
    uint32 u32ScstCumSig = KU32_ZERO;

    u32ScstCumSig = m4_scst_execute_core_tests((uint32) pstScstGrp->Start, (uint32) pstScstGrp->End);

   
    if (m4_scst_accumulated_signature == M4_SCST_TEST_WAS_INTERRUPTED)
    {
          RCM_ResetEcuWithCause();
    }
 
}
 
the definition of test group is bellow:
const mst_stScstGrpDesc_Type mst_castScstGrpDesc[MST_KU8_TESTGROUP_COUNT]=
{
    {   /* Test Group 0 */
        .Start     =          0u,
        .End       =         10u,
        .Signature = 0x55AA52DEu
    },
    {   /* Test Group 1 */
        .Start     =         11u,
        .End       =         18u,
        .Signature = 0xE2498B6Cu
    },
    {   /* Test Group 2 */
        .Start     =         19u,
        .End       =         21u,
        .Signature = 0x660B341Bu
    },
    {   /* Test Group 3 */
        .Start     =         22u,
        .End       =         23u,
        .Signature = 0xC2323B30u
    },
    {   /* Test Group 4 */
        .Start     =         24u,
        .End       =         25u,
        .Signature = 0x9E2102BAu
    },
    {   /* Test Group 5 */
        .Start     =         26u,
        .End       =         31u,
        .Signature = 0x928DDE60u
    },
    {   /* Test Group 6 */
        .Start     =         32u,
        .End       =         33u,
        .Signature = 0x55AAE69Eu
    },
    {   /* Test Group 7 */
        .Start     =         34u,
        .End       =         38u,
        .Signature = 0x15E0123Du
    },
    {   /* Test Group 8 */
        .Start     =         39u,
        .End       =         43u,
        .Signature = 0x980FEBBBu
    }
};
 
The problem is that the test is interrupted in the first test of the table.
Any Idea about how to resolve or diagnostic this problem?
Thank you in advance!
标记 (1)
0 项奖励
回复
3 回复数

1,641 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @aymane_chaib_nxp95,

Can you specify the MCU part and the version of SCST?

 

Thank you,

Daniel

0 项奖励
回复

1,605 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @aymane_chaib_nxp95,

As we have discussed, to avoid problem with SCST tests interruption, the following must be ensured.
1) Execution time for each testgroup must be lower than SysTick timer period.
2) SCST execution shall be synchronized with App SysTick .

 

BR, Daniel

0 项奖励
回复

1,600 次查看
aymane_chaib_nxp95
Contributor I

Hello @danielmartynek ,

 

the solution I adopted was to execute again the test which was interrupted, 5 times maximum, that seems to be a good solution because the interrupted test succeeds after 1 or 2 tries.