S32k324 SysTick

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k324 SysTick

1,681件の閲覧回数
Simone9
Contributor III

Hello,

We are currently developing on MCU s32k324.
I wanted to know if the SysTick peripheral was unique per Core or was only one instance of it in the MCU?
I mean, does each core have a SysTick peripheral or is there only one SysTick in general.

Thank you very much.

0 件の賞賛
返信
1 返信

1,664件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Systick belongs to ARM Cortex-M7 Core. S32K324 has two Cortex-M7 Cores. But the Systick is an optional feature so I'm not sure if it's implemented on every M7 core. (Armv7-M: System Tick Timer)
Sorry, I don't have S32K324 around to test. If it is convenient, you can try to access the Systick of the two cores separately during debugging to see if they exist.


Best Regards,
Robin

0 件の賞賛
返信