S32k1Xx FlexIO timer 16-bit counter mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k1Xx FlexIO timer 16-bit counter mode

ソリューションへジャンプ
2,780件の閲覧回数
yuegao1996
Contributor II

Hi, 

   when i read S32k1 user manual, about flexio timer 16bit counter mode, it says " In 16-bit counter mode, the full 16-bits of the counter and compare register are used to configure either the baud rate of the shift clock or the shifter bit count." 

   dose it mean that the 16bit counter is FFFF at the beginning, and the timer cmp register is used for shifter bit count ?

many thanks.

0 件の賞賛
返信
1 解決策
2,765件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,766件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

0 件の賞賛
返信
2,764件の閲覧回数
yuegao1996
Contributor II

Thanks !

0 件の賞賛
返信