S32k14x FEE configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k14x FEE configuration

2,348件の閲覧回数
pschenke
Contributor II

Application Note "Using S32K148 FlexNVM Memory" describes the several configuration possibilities of the S32K14x EEP support.
The MCAL module FEE needs to be configured to have EEP function in an AUTOSAR project.
There is in both documents nothing mentioned about the configuration specific details.
What should be configured in FEE to have the full support of EEP space with the best possible lifetime support and how is the realtion ship to the falsh sectors to beconfigured in FLS module?

Any help in appreciated.

Peter

タグ(3)
1 返信

2,142件の閲覧回数
pschenke
Contributor II

Solution for the usage of the FlexNvM is using the EEP module of the MCAL package.

This answer was received from the NXP support directly.

The FlexNvM has some HW support, doing the FEE tasks and so the API to the bSW and APP is like an EEPROM.