S32k146 Process expert- No active project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k146 Process expert- No active project

Jump to solution
869 Views
PU1
Contributor II

The  pop up window comes, when I try to generate code . 

I'm am using DS32 ARM 2.2 

pop when try to generate codepop when try to generate code

Also not able to add module to projectwhen try to add module no option is not enablewhen try to add module no option is not enable

0 Kudos
Reply
1 Solution
730 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
712 Views
PU1
Contributor II

Thanks for your reply  @Robin_Shen,

i was following same procedure.

my issue is solved. ,,some packages are not added.

0 Kudos
Reply
731 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that your project is baremetal without SDK included. Please refer to the Attaching an SDK to an existing project of S32DS_ARM_User_Guide.pdf.

Attaching an SDK to an existing project.png

Please select the SDKs next time you create a new project.

Select SDK.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------