S32k146 Evaluation Board Transceiver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k146 Evaluation Board Transceiver

1,651 次查看
marwanibrahim
Contributor II

Hello,

I am using S32k146 evaluation board and i am trying to establish CAN communication.

This is done successfully in case of using CAN 0, if i configure CAN 1, communication is not working.

so my question is , are all CAN peripherals are connected to the transceiver so i can use any CAN instant with any related pin or not?

Can anyone share the evaluation board schematic with me?

0 项奖励
回复
1 回复

1,640 次查看
Jeremy_He
NXP Employee
NXP Employee

Hi marwanibrahim,

Please follow the below link to fetch the SCH, and make sure you have the right version A or B.

Only CAN0 is connected to the transceiver as you can see from the SCH.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3...

146 EVB SCH.png

0 项奖励
回复