S32k144EVB Pinout 3.3V not 5V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k144EVB Pinout 3.3V not 5V

4,229件の閲覧回数
Sorin
Contributor I

Hello,

I am using S32k144EVB (evaluation Board).

I cannot finish my project because I see that for pins from headers J1 and J2, for example PTE3, the logical 1, is 3.3 V. I need 5V.

Is there a way to achieve this?

   

Thank you in advance!

Have a good day,

Sorin

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,896件の閲覧回数
mahmoudsherrah
Contributor III

Yes you can switch your S32K144EVB to work in 5V mode or 3.3V mode.

If you are powering your board through the microUSB port, then by default it should work in 5V mode.

Solution: (assuming you are powering your board through the microUSB port to a PC)

5V Mode:

   - R63 is NOT populated

   AND

   - R64 is populated with 0 ohm resistor OR solder a male 3-pin header to J10 (by default not present) and plug a jumper between 2-3

pastedImage_4.png

-------------------------------------------------------------------------------------------------------------------------------------

3.3V Mode:

   - R64 is NOT populated

   AND

   - R63 is populated with 0 ohm resistor OR solder a male 3-pin header to J10 (by default not present) and plug a jumper between 1-2

pastedImage_1.png

0 件の賞賛
返信

3,896件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Sorin,

If VDD = 5V, log 1 is also 5V at PTE3.

Or do you supply the MCU with 3V3?

Regards,

Daniel

0 件の賞賛
返信