S32k144EVB Pinout 3.3V not 5V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k144EVB Pinout 3.3V not 5V

3,927 Views
Sorin
Contributor I

Hello,

I am using S32k144EVB (evaluation Board).

I cannot finish my project because I see that for pins from headers J1 and J2, for example PTE3, the logical 1, is 3.3 V. I need 5V.

Is there a way to achieve this?

   

Thank you in advance!

Have a good day,

Sorin

Labels (1)
0 Kudos
Reply
2 Replies

3,594 Views
mahmoudsherrah
Contributor III

Yes you can switch your S32K144EVB to work in 5V mode or 3.3V mode.

If you are powering your board through the microUSB port, then by default it should work in 5V mode.

Solution: (assuming you are powering your board through the microUSB port to a PC)

5V Mode:

   - R63 is NOT populated

   AND

   - R64 is populated with 0 ohm resistor OR solder a male 3-pin header to J10 (by default not present) and plug a jumper between 2-3

pastedImage_4.png

-------------------------------------------------------------------------------------------------------------------------------------

3.3V Mode:

   - R64 is NOT populated

   AND

   - R63 is populated with 0 ohm resistor OR solder a male 3-pin header to J10 (by default not present) and plug a jumper between 1-2

pastedImage_1.png

0 Kudos
Reply

3,594 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Sorin,

If VDD = 5V, log 1 is also 5V at PTE3.

Or do you supply the MCU with 3V3?

Regards,

Daniel

0 Kudos
Reply