S32k144 extended ID issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k144 extended ID issue

1,981件の閲覧回数
pritampatil
Contributor III

i am working on FlexCAN module of S32K144.  i am able to transmit and receive CAN frames with standard ID. Here i am facing issue in receiving a CAN frame with extended ID.

I have set IDE bit to 1, still it is not able to receive data.

Sample code has been attached. please look into it.

Regards,

Pritam

0 件の賞賛
返信
1 返信

1,821件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

from the code I do not see you have IDE bit set for the RX MB.

Refer to the attached example. It sets MB4 to receive extended ID = 0x14440000.

Code was changed to use RX interrupt.

Hope it helps.

BR, Petr