S32k clock tolerance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k clock tolerance

1,774 Views
momo12
Contributor III

Hi

I am using the s32k144 evalboard. I am suing the fast internal clock:FIRC

I generated a PWM signal based on FIRC, which is supposed to be 16 Mhz, however it is only 15.6. This gives me more than 2.5 % difference/tolerance.

According to:

https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf 

Table 19.   Fast internal RC Oscillator electrical specifications

There should be only 1%. How comes?

0 Kudos
Reply
1 Reply

1,616 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

It can be a measurement error. I recommend you set PWM with a long period and for example with 50% duty cycle and many pulses. Then do the measurement.

I hope it helps you.

Best regards,

Diana

0 Kudos
Reply