S32K3XX STM timer causing DMA error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3XX STM timer causing DMA error

2,028 Views
Chase1234
Contributor I

I am using an S32K. I have an STM timer that is being initialized in my code that is causing a 37 vector to be activated. This vector is tied to the DMA Channel 17. I was wondering what interactions the STM and the DMA have that could be causing this vector to be active while the DMA is not turned on?

0 Kudos
Reply
3 Replies

1,955 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi @Chase1234,

what is the package's name you are using?

Did you check the interrupt handler function installed for STM interrupt and DMA interrupt?

Could you send me your configuration files (.arxml files)?

Best regards,

Dan

0 Kudos
Reply

1,987 Views
Chase1234
Contributor I

Hi @danielmartynek 

It is the s32k358.

Thanks, Joseph

0 Kudos
Reply

1,992 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Chase1234,

Which S32K3xx part is it?

 

BR, Daniel

 

0 Kudos
Reply