S32K3X4EVB-T172 development board device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3X4EVB-T172 development board device

2,352件の閲覧回数
amitra
Contributor I

Hi,

S32K3X4EVB-T172 development board schematics design file shows 2 NXP processors. S32K358_172MAXQFP_EP(U38) and S32K344_172MAXQFP(U9). Whereas hardware manual specifies only one processor S32K344.

PCB layout brd file has both devices in the same location.

Which device is populated in the development kit.

S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors

Thanks

0 件の賞賛
返信
3 返答(返信)

2,288件の閲覧回数
amitra
Contributor I

If S32K358 is populated in place of S32K344. What other changes are required.

0 件の賞賛
返信

2,279件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@amitra

Specific PCB LAYOUT notes are detailed in ITALICS

for example:

Senlent_0-1679276799138.png

 

0 件の賞賛
返信

2,315件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@amitra

The default should be S32K344, S32K358 is an alternative,
In the schematic diagram, S32K358 is DNP

Senlent_0-1678673135826.png

 

0 件の賞賛
返信