Hi @PavelL,
I was able to run the example TCP/IP stack example project previously with the following configuration:
• S32KDS version 3.6.5
• RTD (Real-Time Drivers) version 7.0.0
• TCP/IP Stack version 4.0.0
However, after upgrading to the following versions and did the same setup procedure, it is not working:
• S32KDS version 3.6.8
• RTD (Real-Time Drivers) version 7.0.1
• TCP/IP Stack version 5.0.0
I have attached my project. Thanks for the help again.