S32K358 - SMR installation for advanced Secure Boot - HSE_SRV_RSP_NOT_ALLOWED

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K358 - SMR installation for advanced Secure Boot - HSE_SRV_RSP_NOT_ALLOWED

3,071 次查看
fp-theophile
Contributor II

Hi, 

I am trying to install a SMR with advanced secure boot mod, I get the following response from the HSE: HSE_SRV_RSP_NOT_ALLOWED. I know it is not related to my LC State, I don't what I am missing. The ECDSA signature for the region is written in internal Flash memory.

Here is my code for the configuration:

hseSmrDecrypt_t smrDecrypt = {HSE_SMR_DECRYPT_KEY_HANDLE_NOT_USED, 0, 0, NULL, 0};
hseEcdsaScheme_t ecdsaScheme = {HSE_HASH_ALGO_SHA2_256, NULL};

hseSignScheme_t cryptoScheme;
cryptoScheme.signSch = HSE_SIGN_ECDSA;
cryptoScheme.sch.ecdsa = ecdsaScheme;

hseAuthScheme_t authScheme;
authScheme.sigScheme = cryptoScheme;

hseSmrEntry_t hseEntry;

hseEntry.pSmrsrc=COM_FLS_u32ActivePhysicalStartAddr;
hseEntry.smrSize = 0X200000U;
hseEntry.pSmrDest = NULL;
hseEntry.configFlags = 0U;
hseEntry.checkPeriod = 0U;
hseEntry.authKeyHandle = 0x00010000U;
hseEntry.authScheme = authScheme;
hseEntry.smrDecrypt = smrDecrypt;
hseEntry.versionOffset = HSE_SMR_VERSION_NOT_USED;

hseSmrEntryInstallSrv_t hseInstallSmr;
hseInstallSmr.accessMode = HSE_ACCESS_MODE_ONE_PASS;
hseInstallSmr.entryIndex = 0u;
hseInstallSmr.pSmrEntry = (HOST_ADDR) &hseEntry;
hseInstallSmr.pSmrData = COM_FLS_u32PassivePhysicalStartAddr;
hseInstallSmr.smrDataLength = 0X200000U;
hseInstallSmr.pAuthTag[0U] = (HOST_ADDR) COM_FLS_u32PhysicalAdressSignature;
hseInstallSmr.pAuthTag[1U] = (HOST_ADDR) COM_FLS_u32PhysicalAdressSignature + 32U;
hseInstallSmr.authTagLength[0U] = HSE_BYTES_TO_BITS(32U);
hseInstallSmr.authTagLength[1U] = HSE_BYTES_TO_BITS(32U);

Regards

 

 

0 项奖励
回复
5 回复数

3,021 次查看
fp-theophile
Contributor II

Hi,

Thank you @VaneB for these documents, I have been through them and did not find anything conclusive

My question was specifically on the error response HSE_SRV_RSP_NOT_ALLOWED, I am not sure about what can cause this error in case of a SMR installation request.

Regards

0 项奖励
回复

3,006 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @fp-theophile 

Please help me check what hseAttrSmrCoreStatus_t is returning.

Also could you verify if the problem is not caused by data cache? This is the most common issue when HSE_SRV_RSP_NOT_ALLOWED is returned even if everything seems to be correct. You can try to disable the data cache completely to check if this is the case.

Otherwise SMR can be erased by service HSE_SRV_ID_SMR_ENTRY_ERASE. Notice that super user rights are needed.

0 项奖励
回复

2,931 次查看
fp-theophile
Contributor II

Hello,

I have only 0s in hseAttrSmrCoreStatus_t.

Also now I have HSE_SRV_RSP_INVALID_PARAM as a response from the hse without changing parameters except trying to change key flags, I don't really know what is going on.

About the cache memory I disabled it so I know it is not the problem. And also I checked I had the user rights.

Regards.

0 项奖励
回复

2,910 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @fp-theophile 

Since hseAttrSmrCoreStatus_t only returns 0, it indicates the following information:

- smrStatus[2U] > [0].bit : 0 - SMR Not verified
                                [1].bit : 0 - SMR verification fail

- smrEntryInstallStatus > 0 - SMR entry not installed

- coreBootStatus[2U] > [0].bit : 0 - Core Not booted
                                          [1].bit : 0 - Core booted with alternate/backup reset address

Have you tried any of the Advanced Secure Boot projects shared above?

0 项奖励
回复

3,049 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @fp-theophile 

To better understand the Secure Boot we provide an application note including demo projects which explains all the steps in detail. It can be downloaded from:
S32K3 Microcontrollers for Automotive General Purpose

Application note can be found here:
Documentation -> Secure Files -> Secure Boot Application note v0.1.1.0 (AN744511)

Associated demo project can be downloaded here:
Design Resources -> Software -> Secure Files -> SecureBootAppNoteDemo (SW745310)

Additionally, example codes are available without RTD that provide different use case scenarios to show the capabilities of the HSE FW. 

S32K3 MCUs for General Purpose HSE Demo Examples

 

BR, VaneB

0 项奖励
回复