S32K358 IPCF TEST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K358 IPCF TEST

2,793 Views
nxpuser007
Contributor I

2.png

Why all IPCF demos are debugged in RAM?

 

0 Kudos
Reply
5 Replies

2,751 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @nxpuser007 

You should be able to find the Debug FLASH into the project's "Debug Configurations" as shown in the image.

VaneB_0-1721081766941.png

BR, VaneB

0 Kudos
Reply

2,740 Views
nxpuser007
Contributor I

微信图片_20240716085754.png

but link file  only  RAM。

0 Kudos
Reply

2,703 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @nxpuser007 

In the S32K3 Inter Platform Communication Framework Version 4.0.0 are provided the linker files for flash.You can use this version as a reference.

0 Kudos
Reply

2,682 Views
nxpuser007
Contributor I

11.png

im used new version IPCF(4.1.0),but not found linker files for flash,Is only version 4.0.0 available?

thank for you help!

0 Kudos
Reply

2,663 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @nxpuser007 

I am afraid it seems that in this IPCF release the linker flash files are only provided for the S32K388 project examples.

0 Kudos
Reply