S32K358 FreeRTOS using multiple cores

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K358 FreeRTOS using multiple cores

1,997件の閲覧回数
nandanchaturbhuj
Contributor I

Hello,

 

I am using FreeRTOS example for S32K358 from Design Studio.

Currently I can execute FreeRTOS on S32K358. 

How can I use multiple cores in FreeRTOS ?

 

I can see start-up code section, 

#define CM7_0_ENABLE                (1)
#ifndef CM7_1_ENABLE
    #define CM7_1_ENABLE            (0)
#endif
#ifndef CM7_2_ENABLE
    #define CM7_2_ENABLE            (0)
#endif

 

But defining "CM7_2_ENABLE" is not making any difference.

Anything more required to enable execution on multiple cores ?

 

 

Best regards,

Nandan Chaturbhuj

 

0 件の賞賛
返信
1 返信

1,973件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately, FreeRTOS doesn't support Multi-cores by default. As a result, there would be no FreeRTOS example on S32K3 Also, I am afraid that it would not be simple to have FreeRTOS on each core of S32K3. However, there are some topics in the Internet that customers can refer to. Here is one of these:

https://forums.freertos.org/t/freertos-and-dual-core/9922

https://forums.freertos.org/t/multicore-advice-and-suggestions/7781

 

0 件の賞賛
返信