S32K344 stops after wdg reset.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 stops after wdg reset.

322 Views
BenjaminKubitschek
Contributor I

Hi,

I am currently about to setup an environment for a S32K344 with the Wdg driver of the SW32K3_S32M27x_RTD_4.4_4.0.0_P20 Mcal.

I perform a somoke-test to test all integrated modules, so I test the wdg too. In the testcase a immidiate reset via the wdg is triggered, but after that the target stays in stop mode (IC5000 Tasking-Debugger).
Now I do not know, if there is something further to configure, that the target does a startup after a wdg reset or if that could be a setting with the debugger.

So I briefly ask for help,


Thank you!

0 Kudos
Reply
1 Reply

283 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @BenjaminKubitschek,

What do you mean by the Stop mode?

Can you read the core register while the MCU is in this state?

Have you tried without the debugger after power-on reset?

The MCU should reset periodically via the WDOG.

 

Regards,

Daniel

 

0 Kudos
Reply