S32K344 interface for 5V SENT protocol signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 interface for 5V SENT protocol signal

266件の閲覧回数
Pinderloo
Contributor I

How do you correct interface the NXP S32K344 for a 5V SENT signal?

AN4856: MPC574xP SENT/SPC Driver – Application Note (nxp.com) gives a very good diagram of the interface, but the S32K344 is a 3V3 powered MCU and so do you need to have a simple voltage divider on 5V SENT signal ?

 

タグ(1)
0 件の賞賛
返信
1 返信

233件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Pinderloo,

S32K344 can be powered by 5V.

If you need it to operate at two voltage levels, you can use the design from the AN or an active voltage level translator, this is down to the user.

 

BR, Daniel

0 件の賞賛
返信