S32K344 data flash size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 data flash size

4,298件の閲覧回数
eiankit
Contributor II

Hi,

This below macro from C40_Ip_cfg.h file. It shows that size of data flash is 256 KB. In reference manual there is memory map attached it showing 128 KB memory.

 

/* Data block addresses */
#define FLS_DATA_BLOCK_BASE_ADDR            (0x10000000U)  /*!< the base address of data block */
#define FLS_DATA_BLOCK_END_ADDR             (0x1003FFFFU)  /*!< the end address of data block */

 

eiankit_0-1636720974626.png

Above image also saying data flash is 128 KB.

So, how much memory I need to consider for data flash memory?

Thanks & Regards,

Ankit Chudasama

タグ(3)
0 件の賞賛
返信
3 返答(返信)

4,255件の閲覧回数
eiankit
Contributor II

Hi @danielmartynek,

Please share update if you have any.

Regards,
Ankit

0 件の賞賛
返信

4,156件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @eiankit,

I'm sorry for the delay.

It should be update in RTD_4.4_S32K3XX_2.0.0.

 

BR, Daniel

 

0 件の賞賛
返信

4,266件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @eiankit,

Thanks for pointing this out.

Let me report that.

 

Regards,

Daniel

0 件の賞賛
返信