S32K344-WB Port Pin Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344-WB Port Pin Configuration

1,152 Views
ekmas-19
Contributor II

I have a few questions on configuring pins for my S32K344-WB board.

  1. For the Siul2_port I could use some help configuring it. Looking at the Siul2_port/PortConfigSet tab, do I need to add an entry for every pin on the MCU being used? I have a total of 78 pins being used, of which 46 pins are SIUL2 type.
    1. if not, what goes on PortConfigSet tab?
    2. if so, how do I go about adding the pins and configuring them?
  1. Each pin also relates to a LLR driver. I have configured the LPSPI driver tab. Do I need to add a driver component for each type on the Pins tab? In other words, I have pins in each of these types, ADC, WKPU, System, JTAG. Do I need to add the corresponding LLR Driver component for each one?
  2. When adding LLR Components from "Add Configuration Component Instance" window, not all components seem to be available. Some have a yellow triangle and a note that "they are not found in the tool chain" How do I resolve that ?
  3. Which Peripherals Component do I add to configure interrupts and ISRs using the LLRs. in the MCAL I think it would be the platform component, but I don't see an equivalent in the LLR Add menu.
Tags (1)
0 Kudos
Reply
1 Reply

1,094 Views
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

1. You should fill the PortPin Mscr value for each pin you have configured in Pins Tool. Since RTD 6.0.0 this step is not necessary. it fills automatically.

_Leo__0-1757352713857.png


2. Regardless of the peripheral configuration in Peripherals Tool. If such signal are routed to an external pad, then it is needed its respective configuration in Pins Tool.
3. You just add them, Update Code and write in main file its respective include.
4. For interrupt configuration use the IntCtrl_Ip driver.

I hope this information is helpful.

0 Kudos
Reply