S32K344: V11 Internal Core logic voltage supply Generation Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344: V11 Internal Core logic voltage supply Generation Issue

988件の閲覧回数
Purushothaman
Contributor I

Hi NXP Team,

We are using the MCU part S32K344NHT1MPBS in our product. Currently our product is in production stage. In production line few boards founded with the issue V11 internal core logic voltage supply is not generated. But, the V25 internal logic is generated.

What is the reason and how to solve this issue?

Waiting for the solution from you.

Thanks,

0 件の賞賛
返信
1 返信

953件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Purushothaman 

Does your schematic follow the recommendations we provided in Figure 25 (Bulk/Bypass and decoupling capacitors scheme for the S32K344 /42 /24 /22 /14 – 172HDQFP) of the Hardware Design Guidelines for S32K3 Microcontrollers, Rev. D6? Make sure the power supply pins are connected correctly.

Also, to check if the problem is due to some issue with the MCU or the custom board, swap one of the non-working MCU boards with a working one. Do you see any change? Is it still not outputting voltage the V11?

 

BR, VaneB

0 件の賞賛
返信