S32K344:Problem occured while downloading the application on target.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344:Problem occured while downloading the application on target.

1,963 Views
fletcher1244
Contributor I

I use simulink for MBD , but I can't download my model into S32K344.

fletcher1244_0-1751426267948.png

Then I tried to connect with JFlash, but still got  errors.

fletcher1244_1-1751426432883.png

There should be no problem with my JLink. I guess the problem lies in the S32K344. Is there any solution?

0 Kudos
Reply
5 Replies

1,935 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @fletcher1244

Are the status LEDs all turning on as shown in the Getting Started guide?

Julin_AragnM_0-1751493392537.png

Are you able to connect through the OpenSDA interface? could this be an issue with the debugger specifically?

Were there any projects previously loaded to the EVB which modifies the watchdog, or keeps the MCU in a reset state?

Best regards,
Julián

0 Kudos
Reply

1,923 Views
fletcher1244
Contributor I

hello,
Thanks for your reply.
Sorry forgot to mention that this board was designed by myself, without OpenSDA interface.
Actually, I have two boards and I can't establish a connection , regardless of whether I have downloaded the project or not. then I try to connect this board through JLINK-commander ,but still reported errors:

fletcher1244_0-1751602796363.jpegfletcher1244_1-1751602806319.jpeg

Do you have any solution?
Thank you.

0 Kudos
Reply

1,904 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @fletcher1244,

I imagine this is not the first attempts to connect to the target. Were you able to connect to them before? Does the board work without the debugger connected? (after reset). The reason for this could be that the board is stuck in a loop from a previously loaded project.

I can also see that the JLink firmware is rather old, could you try updating it (J-Link - Firmware - SEGGER Knowledge Base)? 

Have you tried to attach the debugger while the target is running? There is a community post you can use as reference: Solved: Re: S32K344 with Jlink SWD debug, cannot connect Jlink when MCU crash - NXP Community.

Best regards,
Julián

0 Kudos
Reply

1,870 Views
fletcher1244
Contributor I

Hello,
I tried to update the firmware using JLINK config, but it tells me ‘Not updated, probe/ programmer firmware is already up to date.’

fletcher1244_0-1752116900502.png

I have two boards one of which has no project downloaded, but when I try to connect using JLINK it reports an error (the one below), and it seems like it never connects from the beginning.  So I'm guessing it might not be a software issue, could it be a corrupted chip? (although I don't expect that to be the case). 

fletcher1244_1-1752117024888.png

Do you have any ideas?
Thank you.



0 Kudos
Reply

1,842 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @fletcher1244,

Are both boards custom designs? It could be a HW issue, have you followed the hardware design guidelines from the Hardware Design Package?

Best regards,
Julián 

0 Kudos
Reply