S32K344 Power_Ip_PMC_PowerInit() Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 Power_Ip_PMC_PowerInit() Error

786 次查看
Yown
Contributor II

Hi, I'm having some problems

(RTD Version: SW32K3_S32M27x_RTD_R21-11_4.0.0)

1. Intergrate MCAL Gpt Example to S32DS, and make sure no errors within Build process

Yown_2-1726196144721.png

2. In function Power_Ip_PMC_PowerInit(), after running line 316, the debug process invoke error, during this IP_PMC->CONFIG'value from 0 to 1 

Yown_3-1726196159985.png

 

Yown_4-1726196214764.png

3. Detailed error and EB config

Yown_5-1726196343010.png

Yown_6-1726196397476.png

 

 

 

How can I fix it?

 

0 项奖励
回复
3 回复数

610 次查看
AleCasc95
Contributor II

Has the issue been fixed? I'm experiencing the same issue

0 项奖励
回复

765 次查看
Yown
Contributor II

When i use another example, i found that it enter different switch

Is that means i should change the configuration of GPT examples? 

Yown_1-1726200736298.png

 

 

0 项奖励
回复

715 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Yown,

How do you power the V15 domain of the MCU?

It can be powered directly from an SBC/PMIC or generated by the external ballast VC_BJT.

You need to configure the driver accordingly.

danielmartynek_0-1726582860294.png

 

 

Regards,

Daniel

0 项奖励
回复