S32K344 OTA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 OTA

7,254件の閲覧回数
ZC_Alex
Contributor II

Hi,

I downloaded the S32K3xx OTA Demo installation package SW32K3_OTADEMO_0.8.0_D2203.exe from NXP website, and used the installed original project to verify the HSE function on the S32K344 engineering board.

When I verify the HSE function of the OTA Demo project of S32K344, the error code 0x80 CRYPTO_RET_OPERATION_TIMEOUT is returned for all HSE functions, and the reference manual does not contain reference measures for this problem.How should I troubleshoot this problem?

Thank you all for your help,

Alex

0 件の賞賛
返信
9 返答(返信)

6,342件の閲覧回数
RBSamuel
Contributor III

Hello, Alex!

Were you able to download and install the firmware? I'm facing the same challenge.


Thanks!

0 件の賞賛
返信

7,184件の閲覧回数
zhangsan777
Contributor I

请问哪里可以下载到这个安装包?谢谢

0 件の賞賛
返信

7,132件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

7,233件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alex,

S32K344_HSE_OTA/readme.md mentions that the target device should be an S32K344 with the AB_SWAP HSE firmware installed.

Have you installed the AB_SWAP HSE firmware on the S32K344 engineering board?

S32K344_HSE_OTA AB_SWAP HSE firmware already installed.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

7,227件の閲覧回数
ZC_Alex
Contributor II

Hi Robin,

The project has a Siul2_Port_Ip_Example_S32K344.bin involved in compiling, which I think is AB_SWAP HSE firmware file. According to you, should I download the HSE AB SWAP file such as S32K344_HSE_FW_INSTALL_V_0_1_2_1.elf to the chip first?

Best Regards,
Alex

0 件の賞賛
返信

7,222件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

You should install HSE AB SWAP to the S32K344 first.  Sorry I don't know where you got S32K344_HSE_FW_INSTALL_V_0_1_2_1.elf. As far as I know, 0.1.2.1 is for S32K312(not S32K344). Do you have HSE FW 0.1.1.0 for S32K344?

0 件の賞賛
返信

7,213件の閲覧回数
ZC_Alex
Contributor II

I don't have HSE FW 0.1.1.0 for S32K344.I can't find it on the DocStore.Where should I apply for permission to download this software?

0 件の賞賛
返信

7,205件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

7,028件の閲覧回数
ZC_Alex
Contributor II

Hi Robin,

I can't find how to install HSE AB SWAP in the installation Manual S32K344_HSE_Service_API_Reference_Manual.pdf. Should I download s32k344_hse_fw_1.5.0_2.40.0_pb230807.bin.pink to S32K344 through S32DS software.

Best Regards

Alex

0 件の賞賛
返信