S32K344 MCAL ICU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 MCAL ICU

1,144 Views
Canberk
Contributor II

When configured the ICU peripheral in MCAL I have got errors that I shared down below. I just write include icu  and icu init command in my C  file there is nothing else 

Canberk_0-1680502543431.png

I have got these errors. 

 

in the peripherals section I have got no error. errors accures when I build the code

Canberk_1-1680503389804.png

What should I do is this can be happening because of RTD version.

Thaks a lot

 

0 Kudos
Reply
3 Replies

1,128 Views
Canberk
Contributor II

Thanks for telling me about example. I can build example with 0 error but in the c file Icu_EnableEdgeDetection looks inactive. İs this a problem ?

Canberk_0-1680585441831.png

 

0 Kudos
Reply

1,126 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Canberk,

There is description.txt file in the project, please follow it.

 

Thanks,

Daniel

0 Kudos
Reply

1,131 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Canberk,

Do you use the MCAL ICU APIs or the Ip_ICU APIs?

Can you show the .c file?

There is an RTD MCAL ICU example in the S32DS.

Icu_BlinkLed_ASR_Emios_S32K344

 

Regards,

Daniel

0 Kudos
Reply