S32K344 LOCKTETP_EN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
9,312件の閲覧回数
1260784871
Contributor II

1、Can the S32K344 be configured for dual core use?

2、If yes, how do you configure it? Please tell us the details.

 

0 件の賞賛
返信
1 解決策
9,298件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @1260784871,

A new DCF record with LOCKSTEP_EN = 0 has to be programmed into the UTEST OTP memory.

This can be done using by the C40 IP RTD driver.

First, locate your current DCF record in the UTEST be reading the memory via a debugger.

The first available space (all 0xFF) for a new record should be at 0x1B000768 for a device with the default configuration.

I will send you a simple test project.

 

Regards,

Daniel

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
9,299件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @1260784871,

A new DCF record with LOCKSTEP_EN = 0 has to be programmed into the UTEST OTP memory.

This can be done using by the C40 IP RTD driver.

First, locate your current DCF record in the UTEST be reading the memory via a debugger.

The first available space (all 0xFF) for a new record should be at 0x1B000768 for a device with the default configuration.

I will send you a simple test project.

 

Regards,

Daniel

 

 

0 件の賞賛
返信
8,254件の閲覧回数
FrankLiu2019
Contributor III

The data I read from 0x1B000768 is   D7 2A D5 82 50 00 04 00 D7 2A D5 82 70 00 04 00 D7 2A D5 82 B0 01 04 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF ...So I write a new  record at 0x1B000780.But it didn't work, and the chip was locked

0 件の賞賛
返信
8,278件の閲覧回数
FrankLiu2019
Contributor III

Hi Daniel 

What I read from UTEST does not agree with yours.After I wrote the DCF record to flash, the chip locked.This is my code ,Can you tell me what went wrong.

 How-to-configure-the-S32K344-dual-core-operating-mode 

0 件の賞賛
返信
8,193件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FrankLiu2019,

I see a colleague of mine responded to How-to-configure-the-S32K344-dual-core-operating-mode 

 

BR, Daniel

0 件の賞賛
返信
8,537件の閲覧回数
DrJonM
Contributor III

Hi @danielmartynek 

I would also be interested in your simple test project. Where can O get it?

 

Thanks,

Jon

0 件の賞賛
返信
8,506件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @DrJonM,

Something like that:

#define program_address (0x1B000778)  /* UTEST start address */
#define program_data1 (0x00100004)  /* UTEST DCF Control Word */
#define program_data0 (0x00000100)  /* UTEST Data Word, LOCKSTEP = 0, decoupled*/

/* UTEST Miscellaneous Register */
uint32_t utest_misc_dcf [ ] = {
		(uint32_t)program_data0, /* DCF Data word    8h [0:31]  */
		(uint32_t)program_data1  /* DCF Control word Ch [32:63] */
};

volatile tFLASH_STATUS status;

int main(void)
{
	PFLASH_Unlock(PFLASH_BL5, PFLASH_SS0, PFLASH_S0);

	if((*(uint32_t*)program_address) == 0xFFFFFFFF)
	{
         status = FLASH_Write((uint32_t*)program_address, utest_misc_dcf, sizeof(utest_misc_dcf));
	}
	else{
	    __asm__("NOP");
	}

	for (;;) {
	}
	return 0;
}

 

Regards,

Daniel

0 件の賞賛
返信
7,719件の閲覧回数
ALXY_WANG1
Contributor II
Hi Daniel

Could you send me the project? I also need unlock the S32K344 and tried by myself failed.

Thanks
0 件の賞賛
返信
7,710件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
7,484件の閲覧回数
1260784871
Contributor II

I want to divide the core frequency by 2, after executing the following statement, I can not download the code. May I ask why

1260784871_0-1718448858007.png

 

0 件の賞賛
返信
8,603件の閲覧回数
ZhouPengfei
Contributor III

Hi Daniel

Could you send me the project? I also need unlock the second core and tried by myself failed.

Thanks

0 件の賞賛
返信
7,485件の閲覧回数
1260784871
Contributor II

I want to divide the core frequency by 2, after executing the following statement, I can not download the code. May I ask why

1260784871_0-1718448753536.png

 

0 件の賞賛
返信
9,287件の閲覧回数
1260784871
Contributor II

thanks~

0 件の賞賛
返信