S32K344 GPIO Reset Status Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 GPIO Reset Status Questions

1,643件の閲覧回数
MVR
Contributor V

I'm using an S32K344, 257-pin BGA package.

I would like to understand a little more about the reset status over the pins that we can see in the SK344_IOMUX.xlsx.

1) What does DCF mean?

MVR_0-1692982014501.pngMVR_0-1692982014501.png

 

2) And, if I would like to get the pin state on boot, before reach the "void main(void)" point, would I have to get the "Pad State After Selftest" column, correct?

 

3) Is there a default state for direction (input/output), Driver type (push-pull/pullup...), alternate function and drive strength? 

 

4) What is the difference between DCF and MDM?

 

Thank you!

MVR

タグ(2)
0 件の賞賛
返信
1 返信

1,602件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

A1: PTA2 and PTA3 are allocated to FCCU fault output and PTA5 is for RESET_b. These pins can be configured via DCF records.

S32K344 PTA2 PTA3 PTA5.pngS32K344 PTA2 PTA3 PTA5.png

For FCCU: These pins will behave based on fault protocol used. Refer to chapter 53.3.5 EOUT interface of S32K3XXRM Rev.7.

S32K3xx_DCF_clients Utest DCF Client Register Bits.pngS32K3xx_DCF_clients Utest DCF Client Register Bits.png

A3: See the MSCR reset value of the AC column, which contains these functions.

MSCR Reset value S32K344_IO Signal Table.pngMSCR Reset value S32K344_IO Signal Table.png


Best Regards,
Robin

0 件の賞賛
返信