S32K344 FS26 Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 FS26 Driver

2,518 Views
HT-Habib
Contributor I

I am working on MR-CANHUBK344, I installed SBC FS26 R23-11 6.0.0 and S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.0. I use S32DS.3.6.4., my project is non automotive application, I tried different example and tried to create my own project but I always have the same issue:

After I generate the code, I build the project and I have an error:
#include "CDD_Sbc_fs26.h"  : No such file or directory. 
I am not able to see any functions described in UM34SBC_FS26ASRR23-11 Rev0000R6.0.0 Rev. 6.0
FS26  S32K3 

0 Kudos
Reply
3 Replies

2,397 Views
HT-Habib
Contributor I

Update Code in S32 Configuration Tool is not the solution of my issue. I uninstalled then reinstalled everything even S32DS, then it worked.
thank you for you support

2,390 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Thank you for telling me the solution; I've noted it down.
I'm glad to hear the problem is solved.

0 Kudos
Reply

2,489 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please click Update Code in S32 Configuration Tool Tab before build it.

This project build without error at my side.

If you are unfamiliar with how to import and build projects, please watch the video in the S32k344 example code build error.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply