S32K344 - DIO Configuration support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 - DIO Configuration support

307 Views
Er_AK
Contributor I

MBDT DIO example used and working fine. When used to generate other pin, made the same settings as per the example except port and channel ID. It not generating ant error, but it is not generating output. Is there any document which help to use DIO?

0 Kudos
Reply
1 Reply

299 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, the usage is quite simple here. Are you sure you have device package which supports the pin you would like to configure?

DIO documents are inside the driver package in folder doc.

petervlna_0-1719300961481.png

If you share more details I can try to generate the code for the requested pin.

Best regards,

Peter

 

0 Kudos
Reply