S32K344 CMU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 CMU

2,102 Views
ALXY_WANG1
Contributor II

Currently, we are developing a functional safety module based on S32K344. We need to use S32DS to develop the code for the clock monitoring module. Could you provide sample files to guide the development of CMU_FC and CMU_FU

0 Kudos
Reply
4 Replies

2,085 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ALXY_WANG1,

Some CMUs can be enabled by the MCU MCAL driver.

The driver calculates the thresholds automatically.

danielmartynek_0-1756900431432.png

NXP provides the Safety Application Framework (SAF) for the S32K3xx series, which includes the following sCheck tests:

sCheck_CmuFcTest.c
sCheck_CmuFmTest.c


A development license for the full SAF version is available.

To obtain access please contact your NXP distributor.

 

Thank you,

Regards,

Daniel

0 Kudos
Reply

1,324 Views
ALXY_WANG1
Contributor II

Apart from the sCheck module in SAF conducting fault injection tests, are there any other methods to inject faults into the CMU? Could you provide relevant sample programs? The currently used MCU is S32K344.

0 Kudos
Reply

2,059 Views
ALXY_WANG1
Contributor II
How can it be implemented based on LLD
0 Kudos
Reply

2,033 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ALXY_WANG1,

Although the clock GUI has the following options (RTD 6.0.0):

danielmartynek_0-1756993814885.png

the configurator does not generate code from it, so it is not supported.

 

Regards,

Daniel

 

0 Kudos
Reply