S32K324 -gptp stack version 0.9.0 AS master sometimes send PeerDelayRq package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K324 -gptp stack version 0.9.0 AS master sometimes send PeerDelayRq package

Jump to solution
1,465 Views
Nancy_LAN
Contributor II

dear support.

        the customer used the version of the gptp is 0.9.0,the S32K324 as master, sometimes S32K324 sends PeerDelayRq package. but the PC (Slave) can't respond the PeerDelayRq package. why should master send PeerDelayRq package?

Nancy_LAN_0-1749018682405.png

 

 

       

0 Kudos
Reply
1 Solution
1,377 Views
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

do I understand correctly that the issue is already resolved? Please confirm. 

Please note that NXP gPTP stack (or other IEEE 802.1as implementation) must be operated and correctly configured on each switch in the network for proper functionality. 

In case you need any further support, please let us know. 

View solution in original post

0 Kudos
Reply
3 Replies
1,378 Views
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

do I understand correctly that the issue is already resolved? Please confirm. 

Please note that NXP gPTP stack (or other IEEE 802.1as implementation) must be operated and correctly configured on each switch in the network for proper functionality. 

In case you need any further support, please let us know. 

0 Kudos
Reply
1,416 Views
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

could you please share more info about the setup used? 

E.g., which EVB you're using, what is the counter-device (I guess Linux PC w/ ptp4l?), if there is any switch in between of EVB and PC, maybe a simple schematics of the setup incl. MAC addresses and gPTP roles configured.

Thanks!

0 Kudos
Reply
1,393 Views
Nancy_LAN
Contributor II
Hello janglos,
The hardware board is customers. there is a switch between PC and board.
The customer later reported that it was manually turned off the PeerDelayRq package.
thanks for your support.
0 Kudos
Reply